Container standard attributes

Container standard attributes include:
Container standard attributes
Name
Description
Data Type
Index
PLI Access
ID
Unique Primary Key for a container
Integer
1
Read
Name
Container name
String
2
Read
Controller ID
Integer ID for phase logic programmer to reference this container
Integer
3
Read
Description
Container description
String
4
Read/Write
EU
Engineering Units for measuring the material
String
5
Read
Capacity
The container’s maximum capacity
Real
6
Read/Write
ContainerType
Container Type defines what type of container the user is dealing with. The possible values are:
1=Composite Container
2=Plug-Flow Container
3=Pallet Container
Integer
7
Read
StateID
The ID value that represents the current State of the Container. ID values correlate to the tbContainerState table.
Integer
8
Read/Write
Storage Location
The ID value for the Storage Location (zero if the container is not part of a storage location).
Integer
9
Read
Heel
The value (quantity) of the Container Heel (the amount of inventory that remains in a container after the accessible inventory has been removed).
Real
10
Read/Write
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal