Download data from lot container in use
This request will not download a list of data.
Identifying the lot
The LOT formula parameter does not need to be configured on the phase of the running phase. If the LOT formula parameter is used, it must have the lot name stored in it (either before or after binding occurred). This ensures that the correct lot is referenced. If the lot name is invalid or the material does not exist, the batch is held according to the configured hold propagation setting.
Finding the exact lot from which to get the information is simple for composite and plug-flow containers because only one sublot is accessible at a time. Pallets allow random access to sublots, so that when more than one lot of a material is stored on a pallet, the
FactoryTalk Batch
Server does not know which lot to retrieve data from unless there is only one lot on the pallet or the LOT formula parameter is specified.Configure the PXRQ instruction to download lot data from the current material and current lot within the container the phase is currently running against.
External Request | Data Value Array Element | Value |
|---|---|---|
Download Material Manager Data Container in Use | DINT[0] | 3 |
DINT[1] | Data to download (attribute ID). | |
DINT[2] | The phase parameter tag number the value downloads into. |
Provide Feedback