Download container attributes
Configure the PXRQ instruction in
Logix Designer
to download one attribute of a container to a specified parameter ID. The attribute identified by the attribute ID downloads into the tag specified. Only one value may be downloaded at a time.External Request | Data Value Array Element | Value |
|---|---|---|
Download Material Manager Database Data | DINT[0] | 3 |
DINT[1] | Parameter ID container data downloads to. | |
DINT[2] | Container Controller ID | |
DINT[3] | Attribute ID |
TIP:
The data type in the controller must match the data type of the parameter or report ID specified in the data value array element DINT[1].
Provide Feedback