Cancel a single message
Configure the PXRQ instruction in
Logix Designer
to cancel a single message that was sent to another phase:External Request | Data Value Array Element | Value |
|---|---|---|
Cancel Message to Linked Phase | DINT[0] | message ID |
The request.
FactoryTalk Batch
Server cancels the message associated with the message ID. The message was previously issued using a Send Message to Linked Phase
Provide Feedback