Download on transfer of control

To download values for input parameters configured for download on transfer of control:
Configuration for downloading values for input parameters configured for download on transfer of control
External Request
Data Value Array Element
Value
Download Input Parameters Subset
DINT[0]
2
If the phase associated with the parameters has control strategies enabled, only those parameters belonging to
both
the enabled control strategy and the specified subset are included in the download.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal