Download batch data values

While a batch processes, batch data may be downloaded to a specific parameter. The request must specify the parameter ID to which the batch data is to be downloaded.
IMPORTANT:
The 7600/17600 and 7700/17700 requests are exceptions to the rest of the requests in this category in that they do NOT require specifying the tag to which the data will be stored. Instead, the parameter Min and Max values are downloaded to the actual controller tags associated with the parameters on the phase itself. Note that the Min and Max values are downloaded for ALL the parameters on the phase without exception (including Strings and Enumerations).
The data type of the requested item must match the data type of the specified parameter.
Configure the PXRQ instruction in
Logix Designer
to download
FactoryTalk Batch
data to a specific parameter in the process controller:
PXRQ instruction configuration
External Request
Data Value Array Element
Value
Description
Download Batch Data
DINT[0]
1
Download customer-assigned or automatically-generated batch ID to specified tag number.
FactoryTalk Batch
Server downloads an ASCII – String value.
DINT[1]
parameter ID in which to store the value
Download Batch Data
DINT[0
2
Download unique batch ID to specified tag number.
FactoryTalk Batch
Server downloads an Integer value.
DINT[1]
parameter ID in which to store the value
Download Batch Data
DINT[0
3
Download phase equipment ID to specified tag number.
FactoryTalk Batch
Server downloads an Integer value.
DINT[1]
parameter ID in which to store the value
Download Batch Data
DINT[0
4
Download a value to the specified tag number indicating whether the phase is under recipe control or manual phase control.
FactoryTalk Batch
Server downloads:
0 = Recipe Control
1 = Manual Phase Control
DINT[1]
parameter ID in which to store the value
Download Batch Data
DINT[0
5
Download a value to the specified tag number indicating the current mode of the requesting phase.
FactoryTalk Batch
Server downloads:
0 = P-Auto
1 = O-Auto
DINT[1]
parameter ID in which to store the value
Download Batch Data
DINT[0]
6
Download all phase parameter MIN values to the controller tags associated with those parameters.
Download Batch Data
DINT[0]
7
Download all phase parameter MAX values to the controller tags associated with those parameters.
This request actually downloads values for parameters that do not have
Max
and
Min
values, as defined in
FactoryTalk Batch Equipment Editor
> For example, parameters of type
String
and type
Enumeration
.
For string parameters, the request downloads empty strings.
For enumeration parameters, the request downloads a value of zero (0).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal