Assign data server to phases in unit
When creating a unit, assign a data server to the unit. This data automatically assigns to all phases subsequently created in that unit.
To assign a data server to all phases in a unit:
- Select the unit icon in theDesign Viewarea and selectEdit > Properties. TheEdit Unitdialog box,Generaltab displays.
- From theData Serverlist, select theLogix5000CIP data server that represents the controller connected to all phases created in this unit.

- SelectOK.
Provide Feedback