Select a project file - error messages

If error messages display when selecting a
Logix Designer
, use this table to troubleshoot the issue.
Error messages and recommended actions
Error Message
Action to Take
The specified
Logix Designer
project file was not found.
The file may have been renamed, moved, or deleted after it was selected in the
Select Project File
dialog box.
In Windows Explorer, navigate to the file selected in the
Select Project File
dialog box
,
and verify that it still exists with the same name in the selected location.
No revision of
Logix Designer
is installed.
Logix Designer
is not installed on the same computer as
FactoryTalk Batch Equipment Editor
.
Install
Logix Designer
revision 16.0 or higher on the same computer as
FactoryTalk Batch Equipment Editor
.
The revision of
Logix Designer
required to open the project is not installed.
The installed revision of
Logix Designer
does not support
PhaseManager
functionality.
Upgrade the current installation of
Logix Designer
to revision 16.0 or higher.
The
Logix Designer
project file must be converted. The revision is too old.
The revision of the selected
Logix Designer
project file is lower than revision 16.0.
Open the selected project file in
Logix Designer
revision 16.0 or higher to convert the file to this revision.
The specified file is not a valid
Logix Designer
project file. The file format is not recognized or has been corrupted.
Try to open the selected project file in
Logix Designer
. If it does not open, the file format has been corrupted.
The
Logix Designer
project file is read-only and cannot be opened.
Disable the Read-Only Attribute for the selected project file. In Windows Explorer, navigate to the selected file in the
Select Project File
dialog box. Open the
Properties
dialog box for the file and verify that the
Read-Only
Attribute is not selected.
The
Logix Designer
project file revision does not support phases. Use revision 16.0 or greater.
The installed revision of
Logix Designer
and the selected project file is lower than revision 16.0.
Upgrade the revision of
Logix Designer
to 16.0 or higher. Open the selected project file in
Logix Designer
to convert the file to the upgraded revision.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal