Execute method

The
Execute
method sends an execute command to the
FactoryTalk Batch
Server and retrieves a response string. The
Execute
method applies to the
BatchServer
and
BatchRemote
objects.
Execute method
Syntax
strReturn = object.Execute strExecute
The Execute method syntax has these parts:
Part
Description
object
Object expression that evaluates to a
BatchServer
or
BatchRemote
object.
strExecute
(required) String representing an execute supported by the
FactoryTalk Batch
Server application.
strReturn
Data associated with the specified item. (For the format of this data, refer to the appropriate execute.)
Remarks
The data for the item returns synchronously with this method. The FactoryTalk Batch Server waits, at most, a time period equal to the
TimeoutPeriod
property. If the server does not recognize an item string, then
strReturn
contains FAILED. If the timeout period expires before the data is collected internally to the FactoryTalk Batch Server, then
strReturn
contains TIMEOUT.
This code example is
Visual Basic
6 syntax.
Dimension a
FactoryTalk Batch
Server object and two strings:
Dim svr As New BatchControl.BatchServer
Dim strExecute As String
Dim strReturn As String
svr.TimeoutPeriod = 10000
Format an execute string.
This example asks the
FactoryTalk Batch
Server to acquire resource ID number 1:
strExecute = "ACQUIRE(response,user,0,1)"
Send the execute and print the response:
strReturn = svr.Execute(strExecute)
MsgBox strReturn
Message Box should display "SUCCESS:"
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal