UnitIDBatchID

The
UnitIDBatchID
item lists the operator-entered batch ID for the batch to which the unit belongs.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
UnitIDBatchID
UnitID
is
ASCII - Integer, the
unique Equipment ID corresponding to the unit.
Output Format
The UnitIDBatchID item returns in this format:
<BatchID>
is
ASCII - String (user defined)
This is an example of the return on this request.
A request on
object
.
GetItem(55BatchID)
returns:
Batch_100
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal