UnAcknowledgedEvents

The
UnAcknowledgedEvents
item returns a list of all outstanding operator prompts.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
UnAcknowledgedEvents
Output Format
The UnAcknowledgedEvents item returns in this format:
<UnAckEvents>
is
<NullList>
|
<PromptsList>
<PromptsList>
is
<Prompt>
|
<Prompt>
/crlf
<PromptsList>
<Prompt>
is
<Time>
/t
<BatchID>
/t
<RecipePath>
/t
<Description>
/t
<Event>
/t
<Value>
/t
<EngUnits>
/t
<Area>/
/t
<PCell>
/t
<Unit>/t<Phase>
/t
<UnackedPromptID>
/t
<ParamDataType>
/t
<High>
/t
<Low>
/t
<Default>/t<ActionID>
/t
<HighLimit>
/t
<HighHighLimit>
/t
<HighHighHighLimit>
/t
<LowLimit>
/t
<LowLowLimit>
/t
<LowLowLowLimit>
where:
Field Name
Format
Description
<ActionID>
ASCII - Integer
Action ID as a 32-bit unsigned integer. If non-zero, it is the ActionID of an Ack that is pending for the UnacknowledgedEvent. If zero, then there is no Ack pending.
<HighLimit>
ASCII – Value
High deviation limit for prompts with a <ParamDataType> value of 1 or 2. A value returns when the limit value is defined and a Signature Template is defined, otherwise this field is empty.
<HighHighLimit>
ASCII – Value
High high deviation limit for prompts with a <ParamDataType> value of 1 or 2. A value returns when the limit value is defined and a Signature Template is defined, otherwise this field is empty.
<HighHighHighLimit>
ASCII – Value
High high high deviation limit for prompts with a <ParamDataType> value of 1 or 2. A value returns when the limit value is defined and a Signature Template is defined, otherwise this field is empty.
<LowLimit>
ASCII – Value
Low deviation limit for prompts with a <ParamDataType> value of 1 or 2. A value returns when the limit value is defined and a Signature Template is defined, otherwise this field is empty.
<LowLowLimit>
ASCII – Value
Low low deviation limit for prompts with a <ParamDataType> value of 1 or 2. A value returns when the limit value is defined and a Signature Template is defined, otherwise this field is empty.
<LowLowLowLimit>
ASCII – Value
Low low low deviation limit for prompts with a <ParamDataType> value of 1 or 2. A value returns when the limit value is defined and a Signature Template is defined, otherwise this field is empty.
<Time>
ASCII - String
hh:mm
The time at which the event was generated, as formatted within the Control Panel.
<BatchID>
ASCII - String
Operator-entered batch identification number.
<RecipePath>
ASCII - String
The path within the recipe to the phase where the unacknowledged prompt originated.
<Description>
ASCII - String
A description of the event.
<Event>
ASCII - String
The type of event. Contains the string
Prompt
.
<Value>
ASCII - String
The current value associated with the event. The value will be set to the parameter’s default value until the prompt is acknowledged. For binding prompts, the value will be unit, unitid, unit, unitid.
<EngUnits>
ASCII - String
Engineering units associated with the event, if any. MATERIALS returns for material phase binding.
<Area>
ASCII - String
Area from the equipment database.
<PCell>
ASCII - String
Process cell in which the event occurred.
<Unit>
ASCII - String
Unit in which the event occurred. For binding prompts the unit will contain the alias name.
<Phase>
ASCII - String
Phase in which the event occurred. *
<UnAckedPromptID>
ASCII - String
Unique
FactoryTalk Batch
Server assigned identification number.
<ParamDataType>
ASCII - String
Data type for the response 1=real, 2=long, 3=string, 5=enumeration, 10=binding, 11=binding without material server, 20=phase binding, 21=phase binding without material server.
<MaxValue>
ASCII - String
Maximum allowed value. Not used for binding prompts.
<MinValue>
ASCII - String
Minimum allowed value. Not used for binding prompts.
<Default>
ASCII - String
Default value.
This is an example of the return on this request.
A request on
object
.
GetItem(UnAcknowledgedEvents)
could return:
2/24/2022 4:21:14 PM /t BATCH100 /t 17:FRENCHVANILLA\SWEETCREAMUP:1\SWEETCREAMOP:1 \t EMPCTL:1-1 \t HOLDTIME \t Prompt \t MINUTES \t AREA1 \t NORTHPARLOR \t NPMIXER2 \t NPHEATM2 \t 1 \t 60 \t 5 \t 64 \t 10 \t 20
\t 40 \t 3 \t 2 \t 1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal