StringLabels

The
StringLabels
item returns the labels used for generic strings. There are four groups of five strings. The groups are ordered as follows: Process Cell labels, Unit labels, Phase labels, and Shared Resource labels.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
StringLabels
Output Format
The StringLabels item returns in this format: <StringLabels>
<StringLabels>
is
<ProcessCellLabels>
\crlf
<UnitLabels>
\crlf
<PhaseLabels>
\crlf
<SharedResourceLabels>
\crlf
<ProcessCellLabels>
is
<s1>
\t
<s2>
\t
<s3>
\t
<s4>
\t
<s5>
<UnitLabels>
is
<s1>
\t
<s2>
\t
<s3>
\t
<s4>
\t
<s5>
<PhaseLabels>
is
<s1>
\t
<s2>
\t
<s3>
\t
<s4>
\t
<s5>
<SharedResourceLabels>
is
<s1>
\t
<s2>
\t
<s3>
\t
<s4>
\t
<s5>
where:
Field Name
Format
Description
<s1>
ASCII - String
Label for first generic string.
<s2>
ASCII - String
Label for second generic string.
<s3>
ASCII - String
Label for third generic string.
<s4>
ASCII - String
Label for fourth generic string.
<s5>
ASCII - String
Label for fifth generic string.
This is an example of the return on this request.
A request on
object
.
GetItem(StringLabels)
could return:
Cross Invocation Label 1 English Process Cell \t Cross Invocation Label 2 English Process Cell \t Cross Invocation Label 3 English Process Cell \t Cross Invocation Label 4 English Process Cell \t Cross Invocation Label 5 English Process Cell \crlf
Cross Invocation Label 1 English Unit \t Cross Invocation Label 2 English Unit \t Cross Invocation Label 3 English Unit \t Cross Invocation Label 4 English Unit \t Cross Invocation Label 5 English Unit \crlf
Cross Invocation Label 1 English Phase \t Cross Invocation Label 2 English Phase \t Cross Invocation Label 3 English Phase \t Cross Invocation Label 4 English Phase \t Cross Invocation Label 5 English Phase \crlf
Cross Invocation Label 1 English Resource String \t Cross Invocation Label 2 English Resource String \t Cross Invocation Label 3 English Resource String \t Cross Invocation Label 4 English Resource String \t Cross Invocation Label 5 English Resource String \crlf
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal