ResourceIDOwners

The
ResourceIDOwners
item returns a list of all resource owners and the corresponding owner IDs.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
ResourceIDOwners
ResourceID
is
ASCII - String, the
unique Equipment ID corresponding to a specific resource. A Resource is an equipment entity (Process Cell, Unit, Phase or Shared Resource).
Output Format
The ResourceIDOwners item returns in this format:
<ResourceIDOwners>
is
<NullList>
\crlf |
<OwnsList>
\crlf
<OwnsList>
is
<Resource>
|
<Resource> <OwnsList>
<Resource>
is
<ResourceID>
\t
<ResourceName>
\crlf
where:
Field Name
Format
Description
<ResourceID>
ASCII - Integer
The unique equipment ID configured in
FactoryTalk Batch Equipment Editor
. If the owner is the batch operator, the ID is
0
(zero).
<ResourceName>
ASCII - String
The name of the Process Cell, Unit, Phase or Resource.
This is an example of the return on this request.
A request on
object
.
GetItem(119Owners)
could return:
0 \t OPERATOR \crlf
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal