PhaseIDSS
The
PhaseIDSS
item returns the single step index attribute for a phase or an equipment operation sequence.This table shows the input and output formats for this item.
Format | Description | ||
|---|---|---|---|
Input Format | Request: PhaseIDSS | ||
PhaseID | is | Unique equipment ID corresponding to the phase or equipment operation sequence. | |
Output Format | The PhaseIDSS item returns in this format: <SingleStepText> | ||
Field Name | Format | Description | |
<SingleStepText> | ASCII - String | Value in the Single Step tag in the process-connected device. These are the valid values:
| |
This is an example of the return on this request.
A request on
object
.
GetItem(68SS)
could return:Off
Provide Feedback