IncompleteSignaturesCt
The
IncompleteSignaturesCt
item returns a count of all incomplete signature requests (excluding those generated by private interfaces).This table shows the input and output formats for this item.
Format | Description | |
|---|---|---|
Input Format | Request: IncompleteSignaturesCt | |
Output Format | The IncompleteSignaturesCt item returns in this format: <NumSignatures> | |
where: | ||
Field Name | Format | Description |
<NumSignatures> | ASCII - Integer | Number of incomplete signatures in the batch system (excluding those generated by private interfaces). |
Provide Feedback