EquipmentModelDate
The
EquipmentModelDate
item the timestamp on the equipment model loaded by the FactoryTalk Batch
Server upon startup.This table shows the input and output formats for this item.
Format | Description | |
|---|---|---|
Input Format | Request: EquipmentModelDate | |
Output Format | The EquipmentModelDate item returns in this format: <Date> | |
Field Name | Format | Description |
<Date> | ASCII - String | Time stamp of equipment model. |
This is an example of the return on this request.
A request on
object.GetItem(EquipmentModelDate)
could return:2022.02.24 10:05:16
Provide Feedback