CreateIDEventData

The
CreateIDEventData
item returns the data regarding the most recently generated event for the specified batch.
This table shows the input and output formats for this item.
Input and output formats for this item
Format
Description
Input Format
Request:
CreateIDEventData
CreateID
is
ASCII – Integer, INTERNAL identifier assigned during batch creation. Obtain from the
BatchList
item.
Output Format
The CreateIDEventData item returns in this format:
<EvtData>
is
<SVRSignal>
\crlf
<EList>
where:
<SVRSignal>
ASCII – Integer
0 = continue update of data for this advise
1 = discontinue update of data for this advise
where <EList> is:
<Event>
is
<Event>
|
<Event>
<EList>
<EList>
is
<Time>
\t
<BatchID>
\t
<RecipePath>
\t
<Description>
\t
<EventType>
\t
<Value>
\t
<EngUnits>
\t
<Area>
\t
<PCell>
\t
<Unit>
\t
<EQMName>
\t
<PhaseType>
\t
<UserID>
\t
<CreateID>
\crlf
Field Name
Format
Description
<Time>
ASCII – String
Time at which the event occurred.
<BatchID>
ASCII – String
Operator entered batch identification number.
<RecipePath>
ASCII – String
Procedure identifier from
FactoryTalk Batch Recipe Editor
FactoryTalk Batch Recipe Editor
.
<Description>
ASCII – String
Description of the event.
<EventType>
ASCII – String
Type of event.
<Value>
ASCII – String
Value associated with the event.
<EngUnits>
ASCII – String
Engineering units associated with the event, if any.
<Area>
ASCII – String
Area from the Equipment database.
<PCell>
ASCII – String
Process cell in which the event occurred.
<Unit>
ASCII – String
Unit in which the event occurred.
<EQMName>
ASCII – String
Phase in which the event occurred.
<PhaseType>
ASCII – String
Phase Class Category.
<User>
ASCII – String
Machine Name/User Name of person who issued this event to the
FactoryTalk Batch
Server. This may not be displayed if the event was not generated by the operator.
<CreateID>
ASCII – Integer
Unique batch ID assigned by the
FactoryTalk Batch
Server.
This is an example of the return on this request.
TIP:
A request on
object.GetItem(17EventData)
could return:
2022.02.24 16:20:54 \t BATCH_100 \t 17:MCLS_FRENCHVANILLA\MCLS_SWEETCREAM_UP:1\MCLS_SWEETCREAM_OP:1-1 \t State Changed: \t State Change \t RUNNING \t \t AREA1 \t NORTH_PARLOR \t NP_MIXER2 \t \t \t \t 17 \t \t \t \t \t \t \t \r\n
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal