CPRVersion

The
CPRVersion
item returns data describing the CPR version of the
FactoryTalk Batch
Server.
This table shows the input and output formats for this item.
Input and output formats for this item
Format
Description
Input Format
Request:
CPRVersion
Output Format
The CPRVersion item returns in this format:
<CPR Number>
where:
Field Name
Format
Description
<CPR Number>
ASCII -Integer
CPR number for the release containing this
FactoryTalk Batch
Server version.
This is an example of the return on this request.
TIP:
A request on
object
.
GetItem(CPRVersion)
could return:
9
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal