BatchOverrides

The
BatchOverrides
item returns the number of parameter expression overrides currently in effect for each batch on the batch list.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
BatchOverrides
Output Format
The BatchOverrides item returns in this format:
<Statistics>
is
<NullList>
|
<OverridesList>
<OverridesList>
is
<OverrideRecord>
|
<OverrideRecord>
<OverridesList>
<OverrideRecord>
is
<CreateID>
\t
<NumOverrides>
\crlf
Field Name
Format
Description
<CreateID>
ASCII – String
Integer, INTERNAL identifier assigned by the
FactoryTalk Batch
Server to a batch when created. Obtained from the
BatchList
item.
<NumOverrides>
ASCII - String
Number of overrides in effect for the batch with this CreateID
This is an example of the return on this request.
TIP:
A request on
object.GetItem(BatchOverrides)
could return:
14 \t 3 \crlf
15 \t 0 \crlf
16 \t 5 \crlf
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal