Formulations_Info
The
Formulations_Info
execute retrieves the set of formulations and their descriptions configured within a specified recipe.This table shows the input and output formats for this item.
Execute Format | A FactoryTalk Batch Server supports an execute with this format: [ FORMULATIONS_INFO (<Item>,<UserID>,<RecipeID>)] | |
|---|---|---|
where: | ||
<Item> | Item name as specified by the client. | |
<UserID> | User identification associated with this execute. | |
<RecipeID> | Filename, including the extension, for the recipe for which formulation data is retrieved. | |
Action | A successful FORMULATIONS_INFO execute returns the string "SUCCESS:" followed by a variable number of records, one per formulation defined in the specified recipe. Each record contains the name and description of a formulation defined within the recipe. | |
Return Format | Populates the response item with this data: SUCCESS:<FormDataList> | FAIL:<message> | |
where: | ||
<FormDataList> | is | <NullList> | <FormData> | <FormData> \crlf <FormDataList> |
<FormData> | is | <FormName> /t <FormDesc> /t <FormValid> |
<FormName> | is | Formulation name |
<FormDesc> | is | Formulation description |
<FormValid | is | <Valid> | <Invalid> |
<Valid> | is | "1" |
<Invalid> | is | "0" |
The following is an example of the return on this execute.
Given the following execute:
[FORMULATIONS_INFO(Item,STATION5/operator2,cls_frenchvanilla.bpc)]
The batch server could return:
SUCCESS:PREMIUM/tTOP GRADE/t1/crlfSTANDARD/tOEM BRAND/t1
Provide Feedback