AddEvent_CI

The
ADDEVENT_CI
execute allows an external application to append an event in a
FactoryTalk Batch
electronic batch record file based on its unique CreateID.
The format and return for this execute includes:
Format and return
Format
Description
Execute Format
A
FactoryTalk Batch
Server supports an execute with this format:
[ADDEVENT_CI(
Item,UserID,CreateID,Type,Desc,Value,EU,Cell,Unit,Phase
)]
where:
Item
Response item name as specified by the client.
UserID
User ID entered into the event journal with this event.
CreateID
Unique batch ID assigned by the
FactoryTalk Batch
Server.
Type
Type of event being added.
Desc
Description of the event being added.
Value
Value of the event being added.
EU
(optional) Engineering units associated with the event.
Cell
(optional) Process cell associated with the event.
Unit
(optional) Unit associated with the event.
Phase
(optional) Phase associated with the event.
Action
A successful ADDEVENT_CI
execute places the event into the specified electronic batch record. The
FactoryTalk Batch
Server automatically completes these fields: TIME, AREA, RECIPE, PHASE_DESC, and UNIQUE_ID. If, however, the batch product is configured for signature confirmation of "comments", then adding the event record to the event journal is queued pending successful signoff of a signature request.
Return Format
The item populates with this data:
SUCCESS: | SUCCESS:
<ActionID>
| FAIL:
<message>
where:
Field
Format
Description
<ActionID>
ASCII – Integer
Action ID associated with signature(s) generated as a result of the potential prompt response. The prompt response will not actually be processed unless all signature requests are successfully signed off.
<message>
ASCII - String
Error message appropriately formatted for operator display.
The following is an example of the return on this execute.
An execute string:
[ADDEVENT_CI(Item,Station5\Operator,11,Comment,OperatorComment,This is a comment]
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal