BatchServer object
The
BatchServer
object provides the mechanism used to interact with the FactoryTalk Batch
Server by sending execute commands and
retrieving data items. The BatchServer
object represents the same interface the FactoryTalk Batch View HMI Controls
Library uses for interacting with the FactoryTalk Batch
Server. Thus, all information exposed from the
server application is exposed through this interface.Within a
FactoryTalk Batch
script, a user must dimension a BatchServer
object in order to use the object’s methods and property. This does not start a new instance of the server, but instead represents a new connection to an existing server. Therefore, the server must be running before the user can dimension a new BatchServer
object.The
BatchServer
object is a simple object in that it exposes only two methods and a single property. These methods are GetItem
and Execute
. These map directly to the items and executes documented within this manual. Retrieve any item referenced in this manual through the GetItem
method on the BatchServer
object. Also, send any execute referenced in this manual with the Execute
method on the BatchServer
object. Provide Feedback