FactoryTalk Batch Server API
This information was developed to provide quick and easy access to information regarding
the interface between the
FactoryTalk Batch
Server and FactoryTalk Batch View
— the Application Programming Interface (API). It is a reference for those who want to
develop custom interfaces.The API is the interface between the
FactoryTalk Batch
Server and FactoryTalk Batch View
or a custom user interface application. The server API allows collection of batch control
system information and commands the server to take some action.
TIP:
The interface between the
FactoryTalk Batch
Server and Phase is documented in the .The two basic components of the server API are:
- Items- An item is a named data structure accessed using theGetItemmethod.
- Executes- An execute is a command to theFactoryTalk BatchServer to perform some action.
This diagram depicts the relationships between the various components of a
FactoryTalk Batch
system. The Component Object Model (COM) or Distributed Component Object Model (DCOM)
protocol is used between FactoryTalk Batch View
and the server. Use the COM or DCOM protocol between the FactoryTalk Batch
Server and a custom user interface.
Provide Feedback