Delete a FactoryTalk Batch Server extended property
Extended properties are not available to configure in the user interface. Only
configure them when directed to do so by
Rockwell Automation®
technical support.Each property exists as a pair of strings,
Name
and
Value
.To delete a
FactoryTalk Batch
Server extended
property- OpenFactoryTalk Administration Consoleand sign into theFactoryTalkNetwork Directory.
- InFactoryTalk Administration ConsoleExplorer, do one of the following:
- For a newFactoryTalk BatchServer, right-click the application or the area name and select .
- For an existingFactoryTalk BatchServer, expand the application or the area name, right-click the server, and selectProperties.
- In theFactoryTalk Batch Services Propertiesdialog, select theAdvancedtab.
- In theExtended propertiesarea, select a property from the list and selectDelete.
- SelectYesto confirm the deletion.
- SelectApplyto save the data in theAdvancedtab.
Provide Feedback