Start the FactoryTalk Batch Server service
The
FactoryTalk® Batch
Service Manager communicates with the Windows®
Services of the selected computer to identify
available services. There may be a noticeable delay as communications are
established, marked by the cursor displayed as an hourglass. If the FactoryTalk Batch
Service Manager cannot communicate with the selected
computer's Windows
Services, a message box states that the FactoryTalk Batch
Service Manager failed to connect to the specified
computer.The .
FactoryTalk Batch
Phase Simulator must be running to test FactoryTalk Batch
in a demo environment. For more information, see
The FactoryTalk Batch Phase Simulator
in the FactoryTalk Batch
Administrator's User Manual
, publication BATCH-UM003
IMPORTANT:
The
FactoryTalk Batch
Server cannot start if Security
Authority
is enabled and there is a mismatch between the
Security Authority Identifiers (SAIs) in the area model and the FactoryTalk
Network Directory. For information on your recovery
options, see Troubleshooting
in the .To start the
FactoryTalk Batch
Server service:- In , selectBatch Service Manager. TheBatch Service Manageropens.
- SelectSelect Computer. TheSelect Computerdialog box opens.IMPORTANT:You need administrator privileges to perform this procedure.
- InEnter the object name to select, enter the name of the computer where theFactoryTalk BatchServer is installed, or selectAdvancedto search for a computer.
- SelectOKto close theSelect Computerdialog box.
- From theServicelist, selectFactoryTalk Batch Server.
- (optional) SelectAllow Demo Modeto runFactoryTalk Batchin demo mode. If you runFactoryTalk Batchin demo mode, be aware that theFactoryTalk BatchServer stops after 2 hours of operation.
- Select the method to use for restarting the server after a service halt.
- Cold RestartTheFactoryTalk BatchServer starts in a new instance without restoring data from its previous run. Batches are not added back to the batch list, and operator arbitration states are not recovered. For all batches that were not restored, batch completion events are recorded in theFactoryTalk BatchEvent Journals. After a Cold Restart, you will not be able to resume execution of batches from the previous instance. If Security Authority is enabled, SAIs in a secured area model and any secured recipes must match the current Network FactoryTalk Directory SAI.
- Warm RestartRestarts theFactoryTalk BatchServer and attempts to restore the set of batches that were on the batch list when the server previously stopped. Batch complete events are added to theFactoryTalk BatchEvent Journals for all batches that were not restored to the batch list. After a Warm Restart, any batches that are not restored cannot be recovered or resumed in the future. Batches are restored in Manual execution mode with active transitions in a HELD state. No validation for Security Authority is performed.
- Warm All RestartTheFactoryTalk Batchserver attempts to restart but will not restart if it is unable to restore all the batches to the batch list. If a Warm All Restart attempt fails, the ability to restore batches in the future is not affected. After the issues are resolved, another attempt to restore the batches to the batch list can be made using Warm Restart, Warm All Restart, or Hot Restart. This is the default setting for automatic restarts. Batches are restored in Manual execution mode with active transitions in a HELD state. No validation for Security Authority is performed.
- Hot RestartFollows all the startup rules of Warm All Restart. In addition, theFactoryTalk BatchServer attempts to restore batches to their last known state, including transition states and recipe modes, without any operator interaction.
- SelectStart/Continueto start the service. Wait for the status to change to RUNNING and the light to turn green.
- Select theServer Detailsbutton. TheFactoryTalk Batch Server Detailsdialog box opens.
- InPCD Communications, verify theData Server Statusdisplays the status of the conversation as GOOD.
- SelectStartto begin the tag verification process. When tag verification is COMPLETED, selectOK, or selectStopto end the verification process and then selectOK.TIP:If the number of COM servers exceeds the viewable area within theData Server Statusbox, a scroll bar displays, enabling you to scroll through the list.
- SelectClose. TheBatch Service Managerdialog box closes.TIP:If software component conversation becomesLOSTwhile running in Demo mode, make sure that the simulator is running and try starting the server(s) again.
Provide Feedback