FactoryTalk Batch Windows Firewall exceptions
If the Windows Firewall is enabled when you install applications, the installation program adds the following exceptions to the local
computer:
FactoryTalk
or FactoryTalk
e
ProcedureWindows Firewall Exceptions | |
|---|---|
batchsvr.exe (Batch server installs) | NmspHost.exe |
CodeMeter Runtime Server | OPCEnum.exe |
CodeMeterFWEx1 | Port 1433 TCP ( SQL Server installs) |
DaClient.exe | Port 137 NetBIOS Name Service |
EventClientMultiplexer.exe | Port 135 TCP |
EventServer.exe | Port 80 TCP |
Flexsvr.exe | RDcyHost.exe |
FTCounterMonitor.exe | RnaDiagnosticsSrv.exe |
FTSPVStudio.exe | RnaDiagReceiver.exe |
FTSysDiagSvcHost.exe | RnaDirServer.exe |
iexplore.exe | RsvcHost.exe |
Imgrd.exe | VStudio.exe |
If the Windows Firewall is enabled, and not externally controlled, the does not run automatically, manually run it on each computer in your
Windows Firewall
Configuration Utility
runs automatically during installation. If this utilityFactoryTalk Batch
system after installing servers or clients.To manually run the
FactoryTalk
Windows Firewall Configuration Utility, select Start > Rockwell Software >
Windows Firewall Configuration Utility.
Provide Feedback