Standard viewer message fields in FactoryTalk Diagnostics Viewer

The following is a detailed list of the default
FactoryTalk
Diagnostic Viewer standard message parameters.
Default FactoryTalk Diagnostic Viewer standard message parameters
Field
Data Type
Description
Used In
Message
Variant
Application and event-specific message associated with the event being reported.
If provided by the user, applies to all
FactoryTalk Batch Recipe Editor
and
FactoryTalk Batch Equipment Editor
audit messages.
Severity
Enum
This field specifies the severity of the audit message. This value, along with the Audience parameter, defines where this message is routed.
This is RNADiagSeverity_Info. This is not configurable.
Audience
Enum
This field specifies the audience for the audit message. This value, in conjunction with the Severity parameter, defines where this message is routed.
This is RNADiagAudience_Op. This is not configurable.
Time
Date
Date and time, specified as (GMT/UTC)
Represented in the
TimeStamp
field of the audit message.
Location
BSTR
Name of the host computer.
Represented in the
MachineName
field in the audit message.
Provider
BSTR
Name of the client application or component.
Not used.
User
BSTR
Name of the person logged into the editor.
Represented in the
UserName
field of the audit message.
User Description
BSTR
Fully resolved user name.
Represented in the
UserDescription
field of the audit message.
Args
Variant
Used for
Visual Basic
Compatibility.
Not used.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal