Event Summary report
The Event Summary report displays a custom event summary based on report parameter filter selection. The report displays event records from one event journal based on the Unique ID specified. This report includes a header section and an Event Record Data table. The header displays the specifics of the batch:
The header includes:
Header name | For FactoryTalk Batch , displays | For SequenceManager , displays |
|---|---|---|
Event file name | — | — |
Batch ID | Batch ID | Sequence ID |
Unique ID | FactoryTalk Batch Unique ID | SequenceManager Unique ID |
Recipe Name | Recipe Name | Sequence Name |
Area Name | Area | Controller Serial Number |
Process Cell | Process Cell | Controller Serial Number |
Product Code | Product Code | Blank for SequenceManager |
Product Description | Procedure Description | Extended Text |
Report Status | — | — |
Report Generated By | — | — |
Report Time | — | — |
Row Count | — | — |
Columns in the Event Record Data table can be sorted in ascending or descending order.
Version
The version of the FactoryTalk Batch report provides the following information:
- When the report was last modified.
- The version of the report that is currently installed.
- If a custom report is based on a particular version of a report, it shows which version of the report was used.
Filters
This report features filters for the following:
Filter name | Description |
|---|---|
Start Time | Filters based on start time. Select NULL to filter from the beginning of collected time. |
End Time | Filters based on end time. Select NULL to filter to the end of collected time. |
Batch ID Filter | Accepts search criteria in the form of a Batch Name . Use the asterisk (*) as a wildcard character. |
Process Cell | Filters based on the process cell name or controller serial number. |
Recipe Name | Filters based on the recipe name or the sequence name. |
Unit Name | Filters based on the FactoryTalk Batch unit name or unit ID; or the sequence unit ID. |
Unique ID | Specifies which event records display in the report. |
Event | Specifies which event records to include or exclude in the report based on event type. |
Description | Specifies which event records to include or exclude in the report based on the event description. |
Value | Specifies which event records to include or exclude in the report based on event value, such as recipe header information, scale factor, recipe value change, system message, state change, and so on. |
Columns | Specifies which columns to display in the report. |
Area Name | Users can select all areas or a specific Batch server area name. |
Provide Feedback