Batch Execution report
The Batch Execution report displays an Execution Timeline of a batch. The Batch Execution
report includes Operation Sequences from both
FactoryTalk Batch
and SequenceManager™
events. This report includes a header section and
charts. The header displays the specifics of the batch, such as:Header name | For FactoryTalk Batch, displays | For SequenceManager, displays |
|---|---|---|
Batch ID | Batch ID | Sequence ID |
Unique ID | FactoryTalk Batch Unique ID | SequenceManager Unique ID |
Recipe Name | Recipe Name | Sequence Name |
Area Name | Area | Controller Serial Number |
Process Cell | Process Cell | Controller Serial Number |
Product Code | Product Code | Blank for SequenceManager |
Product Description | Procedure Description | Extended Text |
Formulation Name | Recipe Formulation Name. If formulation parameters are not passed, or are an
empty string, "Default Formulation" displays. | Blank for SequenceManager |
Formulation Description | Recipe Formulation Description. If formulation parameters are not passed, or
are an empty string, the description is empty. | Blank for SequenceManager |
Completion State | — | — |
Start Time | — | — |
End Time | — | — |
Duration | — | — |
Version
The version of the FactoryTalk Batch report provides the following information:
- When the report was last modified.
- The version of the report that is currently installed.
- If a custom report is based on a particular version of a report, it shows which version of the report was used.
Hyperlinks
There is a hyperlink to return to the Batch Listing report. This hyperlink does not pass any parameters back to the Batch Listing report.
Filters
This report features filters for the following:
Filter name | Description |
|---|---|
Start Time | Filters based on start time. Select NULL to filter from the beginning of collected time. |
End Time | Filters based on end time. Select NULL to filter to the end of collected time. |
Batch ID Filter | Accepts search criteria in the form of a Batch Name . Use the asterisk (*) as a wildcard character. |
Process Cell | Filters based on the process cell name or controller serial number. |
Recipe Name | Filters based on the recipe name or the sequence name. |
Unit Name | Filters based on the unit name or the sequence unit ID. |
Unique ID | Specifies which records display in the report. |
Area Name | Users can select all areas or a specific Batch server area name. |
Provide Feedback