Print reports
The Network Editor report printing feature allows you to print network, server, or result pane information, in a report formatted with headers, footers and column headings (in list reports).
To print reports
- In the Network Editor’s Hierarchy pane, select the list or item(s) that you want to print.
- From theFilemenu, clickPrint. You could also click thePrintbutton or press ctrl+p to display thePrintdialog box.
- Ensure that the correct printer is selected, and clickOK.TIP:To configure heading and footer fonts and add a custom footer to your reports, see Set report preferencesSet report preferencesfor instructions.
Provide Feedback