Configure Component Training
Perform the following steps to configure component training:
- Provide the following details inTrainingsection ofConfiguration:
- Output Frequency Min (Hz): Minimum VFD command frequency of the application
- Output Frequency Max (Hz): Maximum VFD command frequency of the application
- Provide the following details inAdvanced Settingssection:
- Training Iterations (Default 100): The number of data trends received from the variable frequency drives from FactoryTalk Analytics GuardianAI. A lower value trains faster but generally results in a lower-quality baseline. The recommended value to use is 100 iterations. The expected time to train the baseline will be 11-18 minutes for each half-hertz increment of the operation frequency.
- Minimum Sample: The minimum number of attributes required by FactoryTalk Analytics GuardianAI. This controls how deviations are detected. Higher value will tend to yield less distinct deviations with more occurrences, while lower value yield more distinct deviations with less occurrences of each. The value ranges from 10 to 60 with values in multiples of five. 10 being the high sensitivity and 60 being the low sensitivity. The default value is 40 and it is optimized for most use cases. Adjust only if there are specific needs.
- Trigger Value Hz (Default Empty): An advanced trigger configured for the drive high-speed trend object. The value set will configure the drive to only send data to FactoryTalk Analytics GuardianAI for training/monitoring when the drive operates at or above the frequency value set for the trigger. This parameter is used for advanced motion-based applications with the variable frequency drive. It will typically not be required when operating FactoryTalk Analytics GuardianAI on pumps, fans, and blowers.
NOTE: The training performance may be impacted when running FactoryTalk Analytics GuardianAI on Windows via a Linux virtual machine. It is also recommended to place FactoryTalk Analytics GuardianAI as close as possible to the drive application to minimize the number of network hops.Configure Training Parameters
- ClickSave. The "Training and monitoring information saved successfully." message is displayed.
- ClickNextto configure the Output Controller.
Provide Feedback