Configure Drive

Perform the following steps to configure a new drive:
  1. On the
    Component Overview
    section, click
    Configuration
    .
  2. Select the desired folder, click
    + Add
    >
    New Drive
    .
  3. Provide the following details in
    Drive
    section of the
    Configuration
    :
    • Select type of drive
      : Select the required type of drive. One of PowerFlex 755, 755HiHP, 755TM, 755TR, 755TL, 755TS, 6000T.
    • Name of drive
      : Provide a unique name for the drive.
    • Drive description
      : Provide a detailed description of the drive. This is optional.
    • Drive Path
      : Provide the drive path.
      Configure Variable Frequency Drive Parameters
      The drive path depends on the network configuration of the drive and the instance hosting FactoryTalk Analytics GuardianAI. If both are on the same network, the drive can be accessible directly via an IP Address. In this scenario, the user can input the drive's IP address.
      IP Address example format
      : 192.168.1.10
      The following illustration depicts the instance that hosts FactoryTalk Analytics GuardianAI and the drive on the same network location.
      Network Illustration of Edge Industrial PC and Drive on the Same Network
      The more likely scenario is the instance that hosts the FactoryTalk Analytics GuardianAI is not on the same network layer as the controller. In this case, the user must input the full CIP path mapping from the controller to the drive.
      CIP Path format
      : {First Bridge Module IP Address}/Backplane/{Second Bridge Module Slot}/2/{Target Drive IP Address}
      CIP Path Example
      : 11.70.20.214/Backplane/2/2/192.168.1.103
      CIP Path Routing Illustration
      The following illustration depicts the instance hosting FactoryTalk Analytics GuardianAI on the control network and the variable frequency drive (VFD) on a subnet.
      Network Illustration of Edge Industrial PC and Drive on Different Networks
      If there are multiple controller networks to connect to a drive, the user must input the full CIP path mapping from the controller to the drive as shown below:
      CIP Path format for 3 networks
      : {BridgeIP}/Backplane/{BridgeModuleSlot}/2/{BridgeIP}/Backplane/{BridgeModuleSlot}/2/{TargetDriveAddress}
      CIP Path Example
      : 10.91.21.168/Backplane/5/2/172.16.1.11/Backplane/2/2/192.168.1.101
      Illustration for CIP Path Routing 3 Networks
    IMPORTANT:
    When running multiple instances of FactoryTalk Analytics GuardianAI, make sure not to reuse a drive path across instances, as this can lead to data conflicts and system instability.
    IMPORTANT:
    FactoryTalk Analytics GuardianAI uses the
    10.0.2.0/24
    subnet internally.
    The Drives or Controllers configured with IP addresses in the 10.0.2.x range (10.0.2.1 through 10.0.2.254) are not supported and cannot be accessed by FactoryTalk Analytics GuardianAI.
  4. Click
    Test Connection
    to verify that the drive is connected and FactoryTalk Analytics GuardianAI can successfully establish and validate the connection.
  5. Click
    Save
    . The "
    Drive Details Updated Successfully.
    " message is displayed.
  6. Click
    Next
    to configure the component details.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal