Utilization view

The Utilization view displays utilization values when online.
Current
Section
Description
Average Current
Displays average of the phase currents in Amps.
L1 current
Displays actual L1 phase current in Amps.
L2 current
Displays actual L2 phase current in Amps.
L3 current
Displays actual L3 phase current in Amps.
Overload
Section
Description
TCU
Displays actual thermal utilization percentage.
Average FLA
Displays actual average current in %FLA.
Application
Section
Description
Trip class
Displays the application trip class setting, which is the value read from physical switch on the device.
FLA
Displays the application overload full-load current setting in amps, this value is read from the physical switch on the device.
Auto reset
Displays the application auto reset enable setting, this value is read from physical switch on the device.
Buttons
Label
Description
Refresh
Manually refreshes data in the view when online with the device. When the button is selected, the AOP reads data from the device by using the CIP explicit messages.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal