Overview screen
This view displays basic information about the device, which was configured in the Device Definition view.
IMPORTANT:
To add a device, choose
Device definition...
.This table describes the 140ME/E100 Overview parameters.
Parameter | Description | ||
|---|---|---|---|
Series | Displays the device series. | ||
Revision | Displays the device revision. | ||
Electronic keying | Displays the keying option for the device. Possible values include:
| ||
Connection | Displays the connection:
| ||
Circuit protector | This field displays the type of circuit protector connected to the communication interface, 140ME or E100 type. Values are:
| ||
Contactor | This field displays the 100-E/104-E-INT-X contactor rating (amps) connected to the communication interface. When catalog "100-E-INT-X" is selected:
When catalog "104-E-INT-X" is selected:
| ||
Controlled by | Displays the control source of the current device configured in the Device Definition view:
| ||
Device Definition | Opens the Device Definition dialog box to configure properties. |
Provide Feedback