Peer Command Configuration Commands

This table displays the list of peer command configuration commands depending on the
Controlled by
parameter for each catalogue. For each settings of
Controlled by
, some peer commands are mandatory to configure and some commands are optional to configure.
Peer command configuration commands
Catalogue name
Controlled by
Supported commands
Remarks
100-E-INT-X
Controller
None
Peer Commands view is not supported when
Controlled by
is set to
Controller
Controller/Peer 2-Wire
Hand
N/A
Off
N/A
Auto
N/A
Reset
Optional
Controller/Peer 3-Wire
Hand
N/A
Off
Optional
Auto
N/A
RunForward
N/A
Stop
N/A
Reset
Optional
Peer 2-Wire
RunForward
N/A
Reset
Optional
Peer 3-Wire
RunForward
N/A
Stop
N/A
Reset
Optional
104-E-INT-X
Controller
None
Peer Commands view is not supported when
Controlled by
is set to
Controller
Controller/Peer 2-Wire
Hand
N/A
Off
Optional
Auto
N/A
RunForward
N/A
RunReverse
N/A
Reset
Optional
Controller/Peer 3-Wire
Hand
N/A
Off
Optional
Auto
N/A
RunForward
N/A
RunReverse
N/A
Stop
N/A
Reset
Optional
Peer 2-Wire
RunForward
N/A
RunReverse
N/A
Reset
Optional
Peer 3-Wire
RunForward
N/A
RunReverse
N/A
Stop
N/A
Reset
Optional
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal