Points view parameters
The
Points
view includes these parameters:
TIP:
These parameters are not available in Run mode.
Parameter | Description |
|---|---|
Off -> On/On -> Off Filter Time | Sets a time by which to delay the transition from Off to On or from On to Off. This feature is useful for filtering out transients in noisy environments. Select a value in milliseconds (ms), in resolutions of 1. The valid range is from 0 through 65 ms. The default value is 1. |
Point | Indicates the point to which the configuration applies. |
Output State During Program Mode | Determines the behavior of each output when the controller transitions program mode. Available values are:
|
Output State During Fault Mode | Determines the behavior of each output when communication with the controller fails. Available values are:
|
Provide Feedback