Logging view parameters
Parameter | Description |
|---|---|
Time-of-use log start day | Displays the current value of time of use (TOU) auto-store day in the
power monitor. The current record for the month is automatically
stored on this day replacing an older record if the log is full. You
may select a different TOU auto-store day using the spinner control.
Select Apply to set in the power monitor.Valid values range from 1 through 31 (default). If offline, the change will take effect when next online. |
Energy log | Use these controls to view and modify the parameters related to
operation of the energy logging function. |
Enable energy log | Determines whether the energy log is enabled. Select the checkbox to
change. Select Apply to set in the power
monitor.If offline, the change will take effect when next online. |
Synchronize energy log with end of demand interval | Indicates the energy log interval is synchronized with the demand
end-of-interval event when the radio button is selected. Select the
other radio button to use a fixed time interval instead. Select
Apply to set in the power monitor.If offline, the change will take effect when next online. |
Energy log interval | Indicates the energy log interval in minutes is displayed in the
spinner control when the radio button is selected. The energy log
interval spinner control is hidden if the energy log interval is
synchronized with the demand interval. When online, use the spinner control to change the energy log
interval. Select the other radio button to synchronize the energy
log with the demand interval. Select Apply to
set in the power monitor.Valid values range from 1 through 60. The default is 15. If offline, the change will take effect when next online. |
Energy log mode | Displays the current energy log mode. The available values are:
Select the desired mode to make a change. Select
Apply to set in the power monitor.If offline, the change will take effect when next online. |
Clear energy log button | Clears the energy log from the power monitor memory and begins a new
energy log when online. This parameter is disabled when offline. |
Clear energy counters button | Clears the energy counters to zero in the power monitor (with
firmware revision 3.0 and later) and begins accumulating energy
anew. This parameter is disabled when offline. |
Provide Feedback