Limits view parameters

The
Limits
view includes these parameters:
Parameter
Description
High Clamp
Choose the desired high clamp limit value.
The range is -32768–32767. The default value for current and voltage is 32767.
High Clamp
is disabled in Run mode.
Low Clamp
Choose the desired low clamp limit value.
The range is -32768–32767. The default value for current and voltage is -32768.
Low Clamp
is disabled in Run mode.
Unlatch
Select to unlatch only the corresponding alarm named to the left of
Unlatch
.
Unlatch
is only available while online.
Disable All Alarms
Select to disable all process alarms.
Disable All Alarms
is disabled in Run mode.
Tip
: Selecting
Disable All Alarms
also disables other features for Limits, such as
Latch Limits Alarms
and
Clamps Limits
.
Unlatch All
and
Unlatch
remain enabled.
Latch Limit Alarms
Select to latch all limit alarms.
Latch Limit Alarms
is disabled in Run mode.
Unlatch All
Select to unlatch all process alarms.
Unlatch All
is only available while online.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal