ChX view parameters (input devices)
The
ChX
view for input devices includes these parameters:Parameter | Description |
|---|---|
Input Type | Indicates the Current Input type. |
Input Range | Specifies the current range as 4–20 mA (default) or 0–20 mA. |
Engineering Units | Shows the unit of measurement for High Engineering and Low Engineering and for the channel’s input value. |
High Signal | Displays the high signal value. |
Low Signal | Displays the low signal value. |
High Engineering | Choose the appropriate scaling high units. Set the value between -32768 and 32767. The default is 16383. |
Low Engineering | Choose the appropriate scaling low units. Set the value between -32768 and 32767. The default is 3277. |
Digital Filter | Specifies the desired filter time constant, in milliseconds (ms). Set the value between 0 (default) and 10,000. |
Provide Feedback