Channels view parameters (output devices)

The
Channels
view for output devices includes these parameters:
Parameter
Description
Channel
Displays the channel number to which this configuration applies.
Output Type
Indicates the Current output type.
Output Range
Specifies the output range for the channel as 4–20 mA (default) or 0–20 mA.
Output Range
is only disabled in Run mode.
Output State During
Program Mode
Choose the program mode. Available values are:
  • Hold Last State
  • Go to Low Clamp (default)
  • Go to High Clamp
  • User Defined Value
Output State During
Fault Mode
Choose the fault mode. Available values are:
  • Hold Last State
  • Go to Low Clamp (default)
  • Go to High Clamp
  • User Defined Value
High Signal
Displays the high signal value.
Low Signal
Displays the low signal value.
Units (Signal)
Shows the unit of measurement for
High Signal
and
Low Signal
.
High Engineering
Indicates the appropriate scaling high values. Set the value between -32768 and 32767. The default is 8191.
High Engineering
is only disabled in Run mode.
Low Engineering
Indicates the appropriate scaling low values. Set the value between -32768 and 32767. The default is 1638.
Low Engineering
is only disabled in Run mode.
Units (Engineering)
Shows the unit of measurement for
High Engineering
and
Low Engineering
and for the channel’s output value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal