Channels view parameters (input devices)
The
Channels
view for input devices includes these parameters:
TIP:
These parameters are not available in Run mode.
Parameter | Description |
|---|---|
Channel | Displays the channel number to which this configuration applies. |
Input Type | Indicates the Current Input type. |
Input Range | Specifies the current range as 4–20 mA (default) or 0–20 mA. |
High Signal | Displays the high signal value. |
Low Signal | Displays the low signal value. |
Units (Signal) | Shows the unit of measurement for High Signal and Low Signal . |
High Engineering | Choose the appropriate scaling high units. Set the value between -32768 and 32767. The default is 16383. |
Low Engineering | Choose the appropriate scaling low units. Set the value between -32768 and 32767. The default is 3277. |
Units (Engineering) | Shows the unit of measurement for High Engineering and Low Engineering and for the channel’s input value. |
Digital Filter | Specifies the desired filter time constant, in milliseconds (ms). Set the value between 0 (default) and 10,000. |
Disable Alarms | Determines whether process alarms are generated.
|
Real Time Sample (RTS) | Choose the real time sample period. The valid range depends on the Notch Filter value chosen. Refer to Notch Filter for this value.The default value is 100. |
Notch Filter | Choose the desired filter frequency for the device. The available values are:
The minimum and maximum RTS values allowed for Notch Filter are:
|
Provide Feedback