Calibration Wizard parameters (output devices)

Calibration Wizard
(output devices) includes these parameters:
Parameter
Description
Channel
Displays the channel number to which this configuration applies.
Calibrate
Identifies the channels for calibration.
Select the checkbox for the channel that you want to calibrate.
Calibration Range
Shows the value currently configured for the channel.
Calibration Status
Shows the status of the calibration per channel as the calibration occurs.
Low/High Reference
Indicates the calibration type.
  • Low Reference
    -
    Shows the value of the low reference signal for the channel.
    The default value is 4.000 mA.
  • High Reference
    -
    Shows the value of the high reference source based on the channel configuration.
    The default value is 20.000 mA.
Recorded Reference
Indicates the measured output values.
For the multimeter accuracy, see the User Manual.
Status
Displays the results of the calibration process:
  • OK
    - Indicates that all the channels calibrate successfully.
  • Error
    - Indicates that channels fail to calibrate. Select
    Retry
    to trigger the calibration process again.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal