Calibration Wizard parameters (input devices)
Calibration Wizard
for input devices includes these parameters:Parameter | Description |
|---|---|
Channel | Displays the channel number to which this configuration applies. |
Calibrate | Identifies the channels for calibration. Select the checkbox for the channel that you want to calibrate. |
Calibration Range | Shows the value of Calibration Range as 4 mA to 20 mA . |
Calibration Status | Shows the status of the calibration per channel as the calibration occurs. |
Low/High Reference | Indicates the calibration type. The low reference is calibrated at a low calibration point and the high reference is calibrated at a high calibration point. Depending upon the mode of calibration (low or high), you must attach the input source to the device. The device reads this value and performs calibration. The low reference and high reference input sources are as follows:
|
Status | Displays the results of the calibration process:
|
Provide Feedback