Calibration view parameters (output devices)

The
Calibration
view for output devices includes these parameters:
Parameters
Description
Channel
Displays the channel number to which this configuration applies.
Calibration Range
Displays the calibration range as
4 mA to 20 mA
.
Calibrate Range
is enabled in Program or Test mode and is only available while online.
Calibration Status
Shows the status of the calibration per channel as the calibration occurs. Valid values include:
  • OK
  • Error
Start Calibration
Select to start the calibration process.
Start Calibration
is enabled in Run mode.
Tip
:
Start Calibration
is available when online.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal