Invalid combination
The
Data Bits
, Parity
, and Stop Bits
values must be one of the following combinations. Refer to this table to modify your configuration, and then apply the changes.Data Bits | Parity | Stop Bits |
|---|---|---|
7 | None | 2 |
7 | Even | 1 |
7 | Odd | 1 |
8 | None | 1 |
8 | None | 2 |
8 | Even | 1 |
8 | Odd | 1 |
7 | Even | 2 |
7 | Odd | 2 |
Provide Feedback