Transmit Data view parameters
The
Transmit Data
view includes these parameters:Parameter | Description |
|---|---|
Termination Mode | Set the channel’s termination mode for transmit data. Valid values are:
|
Termination Delimiter | Set the channel’s terminator delimiter for transmit data using any valid ASCII character. Valid values are:
Termination Delimiter is only available when Termination Mode is set to Exclude Delimiter or Include Delimiter . |
User Defined Value | Specifies a user-defined value for the termination delimiter. If no value is entered in User Defined Value , the termination delimiter is set to Nul . For the supported User Defined Value values and the corresponding configuration tag values, see Supported User Defined Value values. |
Byte Swap Mode | Set to swap bytes with other machines or disable the byte swap mode. Valid values are:
|
Handshake Mode | Sets the handshake mode as Master/Slave (default) or Immediate . |
Provide Feedback