Overview view parameters
The
Overview
view includes these parameters.Parameter | Description |
|---|---|
Series | Displays the device series. |
Revision | Displays the major and minor revision of the device. |
Electronic keying | Displays the electronic keying for the device. |
Connection | Displays the connection type for the device. |
Receive mode | Displays the receive format for the device. |
Transmit mode | Displays the transmit mode for the device. None displays in this field when Connection is set to Listen-Only . |
Data format | Displays the data format for the device. |
Device definition | Changes the definition of the device. |
Parameter | Description |
|---|---|
Maximum number of receive characters | Displays the maximum number of receive characters for the device. |
Maximum number of transmit characters | Displays the maximum number of transmit characters for the device. Maximum number of transmit characters is only available when Connection is set to Data or Enhanced Rack Optimization . |
Provide Feedback