Channel view parameters
The
Channel
view includes these parameters:Parameter | Description |
|---|---|
Baud Rate | Enter the baud rate for the device. Valid values are as follows:
Baud Rate appears shaded in Run mode. |
Data Bits | Enter the data bits as 7 (default) or 8 . |
Parity | Enter the parity as None (default), Even , or Odd . |
Stop Bits | Enter the stop bits as 1 or 2 (default). |
Provide Feedback