ChX view parameters (thermocouple devices)
The
ChX
view for input devices includes these parameters:Parameter | Description |
|---|---|
Input Type | Indicates the Thermocouple input type. |
Sensor Type | Determines the sensor type. Available values are:
|
Input Range | Indicates the input range as -75 mV to 75 mV. |
Temperature Units | Select the temperature type. Available values are:
Temperature Units is only disabled in Run mode. |
Engineering Units | Shows the unit of measurement for High Engineering and Low Engineering and for the channel’s input value. |
High Signal | Displays the high signal value. |
Low Signal | Displays the low signal value. |
High Engineering | Choose the appropriate scaling high units. Set the value between -32768 and 32767. The default value is 1000. High Engineering is disabled in Run mode and when Temperature Unit is set to one of these values:
|
Low Engineering | Choose the appropriate scaling low units. Set a value between -32768 and 32767. The default value is 0. Low Engineering is disabled in Run mode and when Temperature Unit is set to one of these values:
|
Notch Filter | Choose the desired filter frequency for the device. The available values for each channel are:
|
Digital Filter | Specifies the desired filter time constant, in milliseconds (ms). Set the value between 0 (default) and 10,000. |
Provide Feedback