ChX view parameters (input devices)

The
ChX
view for input devices includes these parameters:
Parameter
Description
Input Type
Indicates the input type. Available values are:
  • Current
  • Voltage
Input Range
Choose the current (-IE2C) or voltage (-IE2V) range.
  • The valid ranges for current are 4–20 mA (default) and 0–20 mA.
  • The valid ranges for voltage are 0–10V (default) and -10–10V.
Engineering Units
Shows the unit of measurement for
High Engineering
and
Low Engineering
and for the channel’s input value.
High Signal
Displays the high signal value.
Low Signal
Displays the low signal value.
High Engineering
Choose the appropriate scaling high units. Set the value between -32768 and 32767.
  • The default value for current is 16383.
  • The default value for voltage is 10,000.
Low Engineering
Choose the appropriate scaling low units. Set the value between -32768 and 32767.
  • The default value for current is 3277.
  • The default value for voltage is 0.
Digital Filter
Specifies the desired filter time constant, in milliseconds (ms). Set the value between 0 (default) and 10,000.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal